alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

What Are the Different Types of Tube Fittings?

Multiple types of tube fittings

Your Guide to Choosing the Right Small-Bore Tube Fittings for Your Application

Installation of a small bore tube fittingReliable small-bore fluid systems should be designed and constructed with high-quality components—and one of the most important is the small-bore fitting. Used at critical connection points, fittings should provide leak-tight performance to help you maintain plant safety and operational efficiency.  

There are a variety of types of fittings to choose from, however, and it may not always be clear which is the best choice when you’re performing maintenance on an existing system or building a new one.

Explore training opportunities

How should you choose the right fitting for your needs? Let’s investigate several common fitting types along with their specific characteristics and advantages:

What are Threaded Fittings?

Threaded fittings make a connection by attaching two threaded pieces—the difference between them being male vs. female fittings. Male threads (where threads project on the outside of the fitting) are inserted into female threads (where threads are found inside the fitting).

Straight thread type of tube fittingThreaded fittings come in two distinct varieties: those with straight or parallel threads, and those with tapered threads. Straight threads are designed to hold a nut onto the body of a tube fitting and rely on supplemental items, including gaskets, O-rings, or metal-to-metal contact to create a leak-tight seal. For this reason, straight threads are typically used in applications where system pressure will not exceed 5000 psi.

Tapered thread type of tube fittingTapered threads, meanwhile, are designed to seal as the male and female threads are drawn together. They are constructed at an angle in relation to the centerline, whereas straight threads are parallel to the centerline. A thread sealant or thread tape is required to fill in the gaps between the crests and the roots to prevent system fluids from leaking at the connection. A good sealant will also help prevent galling (a phenomenon where two surfaces in contact seize up as a result of cold welding) during installation. Tapered threads will be effective for system pressures up to 15 000 psi.


System pressure icon

Straight threads are typically used when system pressure will not exceed 5000 psi. Tapered threads are effective for system pressures up to 15 000 psi.


Learn more about thread sizes and pitch

Aside from the noted system pressure limits, the choice between straight or tapered threaded connections is often guided by user preference. Generally, available threaded fittings adhere to common standards; British Standard Pipe (BSP) and the National Pipe Thread (NPT) are two of the most common. It can be beneficial, though, to standardize the use of one type versus the other throughout a facility to reduce potential confusion or misapplication.

What are Compression Tube Fittings?

In contrast to threaded fittings, compression tube fittings (which include the category of ferrule fittings) commonly utilize ferrules to create a leak-tight seal. When the fitting’s nut is tightened, the ferrule is compressed between the nut and the receiving fitting. As a result of this compression, the ferrule firmly and effectively grips the tube, creating a tight seal. The reliability of the tube grip is related to how well the gripping ferrule performs this function. Compression or ferrule fittings also offer the benefit of being simple to assemble and disassemble.

Improved grip strength and seal performance
Compression fittings that feature a two-ferrule design can improve grip strength and seal performance.



What are the Different Types of Compression Types Fittings?

There exist some key design differences among the types of compression tube fittings commonly available today. A bite-type ferrule, as illustrated here in both a single- and double-ferrule design, bows when assembly occurs. This bowing action drives the leading edge of the biting ferrule into the tube to grip or indent the tube surface. The leading edge of these bite-type ferrules is intended to bite for proper tube grip. If there is vibration, pulsation, thermal shock, or side load exerted on the fitting, the minimal contact of the gripping ferrule offers little support behind the bite. This means in a dynamic system, the potential for either damage to the tube or pullout may exist.

Single- versus double-ferrule type tube fittings

Compression fittings that feature a two-ferrule design can improve grip strength and seal performance. Here, a gas seal is created between the front ferrule and the outside diameter of the tubing, as well as between the seal surface of the body. The back ferrule also acts as a primary mechanism to secure the tubing in the fitting. During installation, the back ferrule axially advances the front ferrule and radially applies an effective tube grip.

High vibration resistance

 

Two-ferrule, mechanical grip fittings provide high vibration resistance while maintaining appropriate grip and force.



Medium-pressure mechanical grip type of tube fitting A two-ferrule, mechanical grip design, such as that of the Swagelok® tube fitting delivers hinging-colleting action that can create an even more robust grip and seal. Hinging and colleting action provides more material of the back ferrule in close contact with the tube adjacent to the tube grip. This material provides direct and axial support to the tube gripping function. Additionally, this design reduces the likelihood of fittings backing off in applications where vibration is a concern and allows for a very small amount of movement in the fitting while maintaining the appropriate levels of grip and force. This movement, called “spring back,” creates robust vibration resistance. Additionally, by creating long lines of sealing contact between the ferrules and the tube, this mechanical design creates a highly reliable gas seal. They are a good choice for applications where leak-tight performance cannot be compromised.

Learn more about the Swagelok Tube Fitting advantage

Comparing types of tube fittings

What are Mechanical Grip Fittings?

Medium-pressure mechanical grip fittings—an evolution of two-ferrule compression fittings—also deliver outstanding performance along with enhanced installation efficiency. Swagelok® FK series medium-pressure fittings provide a good example of how mechanical grip technology differs from compression-style fittings. Using similar hinging-colleting action to a standard Swagelok two-ferrule tube fitting, the FK series differs by utilizing a female fitting body, a male nut, and pre-oriented ferrules. This design creates a unique dynamic wedge. The dynamic wedge allows for remakeable pullups by torque and provides gaugeability at initial assembly and remake of the tube fitting. The two-ferrule design creates a more robust grip of the tubing, creating a leak-tight gas seal upon initial installation and every remake.

Swagelok FK series fittings provide a leak-tight seal

FK series fittings additionally feature a pre-assembled cartridge that holds the two ferrules and nut. This helps to ensure proper ferrule orientation and installation. With these features, FK series fittings can help reduce installation time and lower assembly and maintenance costs while providing a more reliable connection, resulting in increased uptime in a variety of applications.

 

Cone and thread type of tube fittingWhat are Cone and Thread Fittings?

Finally, cone and thread fittings are available in a wide variety of alloys and have several design features that make them suitable for medium- to high-pressure applications. Their reliable performance has made them a standard high-pressure fitting choice in a variety of demanding applications for many years.

Cone- and thread-specific tubing, featuring thicker walls and a higher pressure rating, is typically required when cone and thread fittings will be used. A high-performance cone and thread fitting will feature a gland, a collar, a female port, and a weep hole that enables you to detect leaks and verify proper installation.

Cutaway of a cone- and thread type fitting

Special care must be taken when preparing and installing cone and thread fittings. Coning and threading tools are required to make the connection, along with lubricant to reduce friction during the cutting process. The tube must be properly coned and threaded before being joined with the fitting. It’s critical to ensure that no burrs, gouges, or scratches have occurred during the process. Once the tubing prep is complete, a collar is threaded onto the tubing and a gland nut is inserted into the fitting body for final tightening. For systems that experience regular shock or vibration, it is also recommended to use anti-vibration components to help extend the life of the tubing connection. If assembled properly, cone and thread fittings can provide reliable long-term performance in some of the most strenuous fluid system applications.

See a comparison between cone and thread and mechanical grip (FK series) fittings installation.

***

Continue Growing Your Fittings Knowledge

Having learned some of the key differentiators among the types of fitting technologies available today, you will be better equipped to make the right choice for your fluid system applications. However, this article only covers the basics of small-bore fittings—there are many other complexities involved with tube fitting selection and installation. Swagelok tube fitting installation training

If you’re interested in further developing your understanding of the world of small-bore tube fittings, check out Swagelok's in-depth training opportunities. Our training programs provide valuable and practical tools for meeting day-to-day challenges related to fluid system design, operation, and maintenance. Through these in-depth, hands-on courses taught by experienced instructors, both new team members and industry veterans can find the information needed to master tube fitting selection, installation, inspection, and troubleshooting—among other fluid system topics. Learn more about available offerings at the link below.

Let's Talk

Related Fittings Articles

identifying thread size and pitch

An Introduction to Fittings: Identifying Thread Size and Pitch

Learn how to determine thread size and pitch for fittings in your small-bore industrial fluid system using the right tools, decreasing the chance of leaks or blowouts.

Why You Should Not Intermix Tube Fittings

Why You Should Not Intermix Tube Fittings

Learn why intermixing or interchanging tube fitting components from different manufacturers can lead to poor fluid system performance.

Swagelok cng lng fittings

Specifying High Performance CNG/LNG Fittings

Compressed natural gas (CNG) and liquefied natural gas (LNG) transportation applications require high-performance tube fittings that meet a number of important criteria. Learn what makes for an ideal CNG fitting or LNG fitting.