What is Return Pressure, What Affects It, and Why Does it Matter?
There are many factors to consider for liquid sampling. That's why we put together a five-part Ask Swagelok video series that discusses the importance of maintaining proper vapor space compression, the role of outage tubes, how vapor space is affected by sampling system design, and what you need to know to minimize the risk of cylinder rupture.
In the fourth video, fluid sampling expert Matt Dixon explains return pressure and why it matters in liquid sampling.
Video Transcript
LUCAS TREU:
Hi there. I'm Lucas Treu, and this is Ask Swagelok. I'm at the Solon Tech Center today with Matt Dixon, one of our sampling system experts, and we're talking about liquid sampling—specifically into cylinders. So Matt, when we talk about cylinder sampling, what is return pressure, what affects it, and how does it impact the sample?
MATT DIXON:
In addition to the return pressure coming from the process itself, there may also be components installed downstream of the sample cylinder—things like a check valve or a back‑pressure regulator. These components add additional backpressure onto the cylinder, and that pressure is essentially additive to the return pressure.
The effect is that you end up with a higher return pressure on the top side of the cylinder. Ironically, or maybe counterintuitively, that actually increases the size of the vapor space. It does this by ensuring that more of the gas initially inside the cylinder stays there rather than escaping. The more gas that remains, the better it can maintain the vapor space after the liquid sample is trapped in the cylinder.
LUCAS TREU:
All right. Well, thanks, Matt. And thank you all for joining us for Ask Swagelok.