alert icon

Internet Explorer 8 or 9 is not supported by this website. Please use a more up to date browser.

Hide Message hide icon

Keep Construction Moving—Without Costly Rework

During active installation, small issues can quickly become schedule risks. Swagelok works alongside your team onsite to identify and resolve problems early so work stays on track.

Connect with your local team

Keep Construction Moving—Without Costly Rework

During active installation, small issues can quickly become schedule risks. Swagelok works alongside your team onsite to identify and resolve problems early so work stays on track.

Connect with your local team

 Back to Global Construction


Construction Phase Services and Onsite Support for Upstream Oil and Gas Projects and FPSO Installation


Construction iconDuring construction, execution is everything—and construction phase services play a critical role in ensuring installation quality, reducing rework, and maintaining schedules across upstream oil and gas projects. Crews are installing, systems are taking shape, and small issues can quickly become schedule risks if they aren’t addressed at the moment they appear.

From onshore builds to offshore applications such as FPSO installation, execution is everything. This is where Swagelok supports you—working alongside your team onsite to help keep installation moving, protect quality, and reduce rework as the project progresses. As part of Swagelok global construction services, this support integrates with teams across project phases to maintain consistency and execution quality.

Find local, global support

  line

What Are Construction Phase Services in Upstream Oil and Gas?

Construction phase services support installation, inspection readiness, and execution during the active build phase of a capital project. In upstream oil and gas construction, these services help reduce rework, maintain quality, and ensure systems are installed correctly before commissioning and startup.

Onsite Construction Phase Services for Installation and FPSO Projects

Location pinWhen Swagelok is engaged during construction, we don’t support the project from a distance. We are present at the jobsite, working directly with your team as installation unfolds. This is especially important in complex environments such as FPSO installation, where installation accuracy and coordination directly affect commissioning and startup performance.

Our specialists collaborate with owners, EPCs, and package vendors to help interpret specifications, resolve constructability challenges, and support proper installation practices—especially where small‑bore fluid systems are involved, including complex applications such as FPSO installation. When questions arise during fit‑up or assembly, we help address them in real time, before work is closed in or needs to be undone.

Being onsite also allows us to support inspection and testing activities as they happen. We help crews prepare for hydrotesting and inspections, verify installation practices ahead of critical milestones, and align documentation with your QA/QC and compliance requirements. This hands‑on involvement helps reduce late‑stage corrections and keeps work moving forward.

Construction Phase Support for Material Flow and Jobsite Continuity

Process iconConstruction schedules depend on material being available when crews need it. As work progresses, conditions change—and shortages or damaged components can disrupt momentum.

Swagelok supports you during construction by helping manage material availability at the jobsite. This includes supporting bulk material needs, addressing top‑up requirements as installation continues, and helping teams manage overages, shortages, and damages. The goal is simple: minimize downtime and keep crews productive without unnecessary delays.

Field engineer verifying proper industrial fluid system installationConstruction Phase Services That Support Commissioning and Startup

The way systems are installed, verified, and documented during construction directly affects commissioning, startup, and long‑term operation. Our construction phase support is designed with that continuity in mind.

By working with you during active installation, we help deliver systems that are ready for the next phase—reducing rework, supporting a smoother transition into commissioning, and setting up the project for successful startup.

What to Expect from Construction Phase Services

  • Onsite technical support to keep installation moving
  • Real-time resolution of constructability challenges
  • Improved installation quality and reduced rework
  • Better preparedness for inspection, testing, and commissioning
  • Reduced schedule risk through material and execution support

What Support Is Needed During Construction in Upstream Oil and Gas Projects?

Support iconUpstream construction projects require onsite technical support, installation guidance, material coordination, and inspection readiness to ensure systems are installed correctly and prepared for commissioning and startup.

What Are Construction Phase Services in Upstream Oil and Gas?

Construction phase services support installation, inspection readiness, and execution during the active build phase of a capital project. In upstream oil and gas construction, these services help reduce rework, maintain quality, and ensure systems are installed correctly before commissioning and startup.

Onsite Construction Phase Services for Installation and FPSO Projects

Location pinWhen Swagelok is engaged during construction, we don’t support the project from a distance. We are present at the jobsite, working directly with your team as installation unfolds. This is especially important in complex environments such as FPSO installation, where installation accuracy and coordination directly affect commissioning and startup performance.

Our specialists collaborate with owners, EPCs, and package vendors to help interpret specifications, resolve constructability challenges, and support proper installation practices—especially where small‑bore fluid systems are involved, including complex applications such as FPSO installation. When questions arise during fit‑up or assembly, we help address them in real time, before work is closed in or needs to be undone.

Being onsite also allows us to support inspection and testing activities as they happen. We help crews prepare for hydrotesting and inspections, verify installation practices ahead of critical milestones, and align documentation with your QA/QC and compliance requirements. This hands‑on involvement helps reduce late‑stage corrections and keeps work moving forward.

Construction Phase Support for Material Flow and Jobsite Continuity

Process iconConstruction schedules depend on material being available when crews need it. As work progresses, conditions change—and shortages or damaged components can disrupt momentum.

Swagelok supports you during construction by helping manage material availability at the jobsite. This includes supporting bulk material needs, addressing top‑up requirements as installation continues, and helping teams manage overages, shortages, and damages. The goal is simple: minimize downtime and keep crews productive without unnecessary delays.

Field engineer verifying proper industrial fluid system installationConstruction Phase Services That Support Commissioning and Startup

The way systems are installed, verified, and documented during construction directly affects commissioning, startup, and long‑term operation. Our construction phase support is designed with that continuity in mind.

By working with you during active installation, we help deliver systems that are ready for the next phase—reducing rework, supporting a smoother transition into commissioning, and setting up the project for successful startup.

What to Expect from Construction Phase Services

  • Onsite technical support to keep installation moving
  • Real-time resolution of constructability challenges
  • Improved installation quality and reduced rework
  • Better preparedness for inspection, testing, and commissioning
  • Reduced schedule risk through material and execution support

What Support Is Needed During Construction in Upstream Oil and Gas Projects?

Support iconUpstream construction projects require onsite technical support, installation guidance, material coordination, and inspection readiness to ensure systems are installed correctly and prepared for commissioning and startup.

line

Construction Phase Support for EPCs and Upstream Project Teams

Globe iconSwagelok supports the teams responsible for making construction happen—EPCs and contractors managing daily execution, owner/operators focused on quality and long‑term reliability, and project teams preparing for commissioning and startup.

We integrate with your jobsite during active construction, providing on‑site technical support, installation guidance, material coordination, and inspection readiness that helps you keep work moving and avoid unnecessary rework. Our global network of sales and service centers scales to match your project’s complexity, location, and pace—meeting you where the work is happening.

If you’re looking for a partner who understands construction realities and supports execution onsite, we’re ready to work alongside your team.

Talk with us about construction phase support and how Swagelok can help you execute with confidence—from installation through the transition to commissioning.

Connect with Us

line

Construction Phase Support for EPCs and Upstream Project Teams

Globe iconSwagelok supports the teams responsible for making construction happen—EPCs and contractors managing daily execution, owner/operators focused on quality and long‑term reliability, and project teams preparing for commissioning and startup.

We integrate with your jobsite during active construction, providing on‑site technical support, installation guidance, material coordination, and inspection readiness that helps you keep work moving and avoid unnecessary rework. Our global network of sales and service centers scales to match your project’s complexity, location, and pace—meeting you where the work is happening.

If you’re looking for a partner who understands construction realities and supports execution onsite, we’re ready to work alongside your team.

Talk with us about construction phase support and how Swagelok can help you execute with confidence—from installation through the transition to commissioning.

Connect with Us