What are PFAS? Understanding PFAS in Swagelok Products
Expert Insights on PFAS in Swagelok Products: Making Informed Material Choices
If you’ve been following news about industrial materials or environmental regulations, you’ve likely heard the term “PFAS” mentioned with growing frequency. But what exactly are PFAS, and why are they drawing so much attention? As principal materials engineer at Swagelok, I’m here to help demystify PFAS, explain their role in our products, and guide you in making informed choices for your applications.
What are PFAS and why do they matter?
PFAS is the acronym for “per- and polyfluoroalkyl substances.” This is a large family of thousands of substances that contain the element fluorine. The unique characteristics of fluorine (i.e., small atomic radius, extreme electronegativity) are responsible for the formation of substances such as gases, chemicals, and polymers having remarkable properties. These properties include unusual stability, extreme heat and chemical resistance, water repelling, oil repelling, and low friction making fluorinated substances useful in a wide range of applications. Fluorinated substances are used in nearly all industries including electronics, semiconductors, textiles, apparel, automotive, aerospace, defense, firefighting foams, oil & gas, construction, food packaging, medical, pharmaceutical, energy, and waste management.
Why are PFAS under scrutiny?
Select fluorinated chemicals, perfluorooctanoic acid (PFOA), perfluorooctanesulfonic acid (PFOS), perfluorohexanesulfonic acid (PFHxS), perfluorononanoic acid (PFNA), hexafluoropropylene oxide dimer acid (HFPO-DA), have been linked to health hazards either due to toxicity or bioaccumulation. Globally, several contaminated sites have been identified. These contaminated sites are primarily located near industrial and waste management sites or near military sites and airports where PFOS is used in firefighting foams. Today, these select chemicals are either banned from use or heavily restricted in drinking water in nearly all industrial countries. Although these select chemicals are already banned or restricted, there is a concern that similar fluorinated chemicals could be synthesized that would also pose a health risk.
Are there other concerns surrounding PFAS?
Yes, since fluorinated substances are stable (meaning that they do not break down easily) there is a concern that fluorinated substances will accumulate in the environment. This is why fluorinated substances are sometimes referred to as “forever chemicals.” Innovative methods to break down fluorinated substances using biological methods that utilize microbes and enzymes to break down these materials, photocatalysis and other forward-thinking approaches are being researched to ensure safe, sustainable and cost-effective methods to address this concern.
Responsible Manufacturing
In addition to managing the end of life of fluorinated substances, all major European manufacturers of fluorinated substances, including AGC Chemicals, Arkema, The Chemours Company LLC, Daikin, Syensqo SA, and W. L. Gore & Associates , have voluntarily committed to a responsible manufacturing program that aims to reduce the emissions of non-polymeric fluorinated substances to 0.003% to air and 0.0006% to water by the end of 2030. Due to advancements in polymerization aid technology, these manufacturers have already achieved the first milestone of emission reductions of 0.009% in air and 0.001% in water. You can learn more about the commitment to responsible manufacturing by following the Fluoropolymers Product Group of Plastics Europe (https://fluoropolymers.eu/).
The American Chemistry Council also administers an organization, Performance Fluoropolymer Partnership (PFP), that has the mission to promote the responsible production, use, and management of fluoropolymers, while also advocating for a sound science- and risk-based approach to regulation. Members of PFP include 3M, AGC Inc., The Chemours Company LLC, Daikin America, Inc., Groupe SEB, Gujarat Fluorochemicals Limited, Honeywell, MilliporeSigma, Shamrock Technologies, Sherwin-Williams, Syensqo, T-Lon Products Inc., Teadit, W.L. Gore & Associates, and Zeus Company Inc. PFP’s website (https://fluoropolymerpartnership.com/) has a wealth of information regarding fluoropolymers and their socioeconomic importance, fluoropolymer uses, and safety & regulations.
Is the use of fluorinated substances always necessary?
No, although fluorinated substances offer advanced performance, you may want to consider the difference between essential and non-essential uses. For many demanding applications, especially those requiring resistance to high temperature and aggressive chemicals, there simply is no acceptable alternative. Non-critical (non-essential) applications that do not require the unique properties of fluorinated substances provide opportunities to consider alternatives. Alternatives are already being adopted for non-essential uses such as ski wax and baking paper.
PFAS in Swagelok products—What you need to know
Swagelok does not use any of the currently banned or restricted fluorochemicals (perfluorooctanoic acid (PFOA), perfluorooctanesulfonic acid (PFOS), perfluorohexanesulfonic acid (PFHxS), perfluorononanoic acid (PFNA), hexafluoropropylene oxide dimer acid (HFPO-DA)) in its products. Fluoropolymers are very different than fluorochemicals. Science-based evidence indicates that fluoropolymers are non-toxic, non-mobile, and non-bioavailable. Fluoropolymers are essential for demanding industrial applications where employee and environmental safety or system performance is critical. To meet these needs, many of Swagelok’s products use fluoropolymers in soft seals and seats because they enable high temperature and chemical resistance. For customer systems with demanding environments, these properties are critical for safety and performance.
Watch Marcy clarify concerns about PFAS in Swagelok products.
(+) View transcript
Matt Ferraro (Product Manager):
Have you ever wondered what PFAS are or what products contain them? Then join us for this Ask Swagelok video.
My name is Matt Ferraro, Product Manager, and I'm here with Marcy McQuary, Principal Materials Engineer at Swagelok.
Marcy, we’ve heard the term “PFAS” thrown around a lot lately. What does that mean?
Marcy McQuary (Principal Materials Engineer):
PFAS is the abbreviation for per‑ and polyfluorinated alkyl substances. In simple terms, it refers to thousands
of chemicals that contain the element fluorine. What’s important to understand is that only about 10% of those
fluorinated chemicals are used commercially.
Matt:
So what are the concerns surrounding PFAS that are driving all this regulatory scrutiny?
Marcy:
There are a few fluorinated chemicals with very low molecular weight that have been linked to health hazards.
Those materials are already heavily regulated. They are very different from the materials used in Swagelok
products—specifically fluoropolymers, which have very high molecular weight. These high‑molecular‑weight
materials have not been linked to health hazards.
However, another concern is that these materials don’t break down easily. They’re often referred to as “persistent,” and that’s part of the broader discussion around PFAS.
Matt:
Can you expand on that? What types of PFAS are used in Swagelok products?
Marcy:
Fluoropolymers are key to our soft seals and seats. They enable high‑temperature ratings and extreme chemical
resistance, which are critical for many customer applications. Importantly, we do not use the
low‑molecular‑weight PFAS that are heavily regulated. We only use high‑molecular‑weight fluoropolymers that
have not been linked to health hazards.
Matt:
That’s good to hear. Does Swagelok offer any products that do not contain PFAS?
Marcy:
Yes. We offer options. For customers who need high‑temperature performance and extreme chemical resistance,
we provide soft seals and seats made from materials such as FKM, FFKM, PTFE, and PCTFE. These materials deliver
the required performance.
For customers whose systems do not require high temperatures or aggressive media compatibility, we also offer alternative soft‑seal and seat materials that do not contain fluoropolymers.
Matt:
How are fluoropolymer manufacturers responding to these concerns?
Marcy:
All major fluorochemical manufacturers have committed to responsible manufacturing practices, including
stringent emission‑control standards. They’ve invested heavily in these improvements. Many are also working
to eliminate fluorosurfactants from their products, which helps remove the PFAS types associated with
health hazards.
Matt:
If customers have questions or concerns about PFAS in Swagelok products, what should they do?
Marcy:
They should contact their local Swagelok Sales and Service Center. They can help customers understand which
PFAS‑containing materials are used in our products and assist with selecting the best materials for their
applications. Customers can also visit swagelok.com to locate their
nearest Sales and Service Center.
Matt:
Marcy, thank you so much for your time and expertise.
Marcy:
You’re welcome, Matt.
Matt:
And thank you for joining us for this episode of Ask Swagelok.
Options for Customers Who Want PFAS Alternatives
Which fluoropolymers are used in Swagelok products?
Fluoropolymers such as FKM, FFKM, PTFE, PFA and PCTFE are key to Swagelok’s product performance. These materials are the standard seat and seal materials in many of Swagelok’s products because they enable a high temperature rating of 400 °F (204 °C). Without these materials, the high temperature product ratings would drop to nearly half of this temperature rating. These fluoropolymers also provide elevated chemical resistance to a wide range of aggressive chemicals including acids such as hydrochloric acid and nitric acid, solvents such as toluene and benzene and many other chemicals that are too aggressive for non-fluorinated materials. For customers who need these capabilities, fluoropolymers are often the best, and sometimes the only choice.
How Swagelok Can Help You Select the Right Product
Choosing the right product for your application can be complex, especially when considering factors like chemical resistance, temperature ratings, and regulatory requirements. That’s where Swagelok’s expertise comes in. Our team of materials engineers and product specialists are ready to help you understand which PFAS materials are used in our products and guide you toward the safest, most effective solutions for your needs.
If you have questions or concerns about PFAS in Swagelok products, we encourage you to contact your local Swagelok sales and service center. Our experts can help you navigate product selection and ensure you have the information you need to make confident decisions.