Understanding Pressure Regulator Performance
Pressure regulator performance plays a critical role in maintaining safe, reliable, and efficient fluid system operation. A regulator must consistently respond to changing system conditions—including fluctuations in flow, temperature, and pressure—to deliver accurate pressure control and help prevent disruptions to system performance. When regulators do not perform as expected, the result can be reduced efficiency, maintenance challenges, or potential safety concerns.
In this video, Swagelok product managers and field engineers explain the key factors that influence regulator performance, including accuracy, robustness, maintainability, and proper application selection. You'll learn how regulator design features, such as seat materials, integrated filtration, spring range, and serviceable components, can affect long-term reliability and ease of maintenance. The video also highlights the importance of selecting the right regulator for your specific operating conditions and how local technical support can help optimize system performance. Understanding these principles can help improve regulator longevity, enhance system reliability, and support safer fluid system operation.
Video Transcript
The basic function of a regulator is to consistently and reliably control pressure for a system. If the regulator doesn’t perform as the customer expects, they will see an interruption to the system in which the regulator has been placed. It has to function properly to ensure the customer’s system functions as it should. Safety is an important aspect of the regulator. When a regulator does not perform properly and fluid escapes into the atmosphere, it can result in a safety issue for the operator.
If a regulator is working, many of the things we see in the field as it operates are related to that regulator’s accuracy. What that means is, as one thing in the system changes, whether it is flow rate, a temperature change, or even the sun going down and it getting cool outside, you can have subtle changes in the system that will affect pressure delivery. The accuracy of a regulator is judged by how well it deals with all of those changes.
Very often, when our customers think about the quality of regulators, they are thinking about robustness. That is the ability for the pressure regulator to continue doing its job, even with all the things that a fluid system can throw at it, like contamination or chemical attack, things that can cause a regulator to stop functioning. The way that Swagelok has designed and built our regulators has robustness in mind. Our seat designs and materials are built in such a way that they can deal with a level of contamination before needing maintenance that some others might not.
Integrated filters for those really dirty systems help prolong the life of those pressure regulators as well. This series of regulator has a longer-range spring, which allows for better resolution while we are adjusting the control pressure. The benefit of a larger-range spring is that it is easier for the customer to dial in the outlet pressure they are intending, instead of having a shorter-range spring, which is more sensitive to adjustments to the handle.
Swagelok is known for its quality and reliability. Our design sophistication and testing allow us to ensure that regulators will perform in real-world applications. We have an extreme level of test equipment, so we can make our own flow curves, and every regulator we supply into the market is 100% tested with our own test equipment. Some people think that it stops at that point, but we also have a system where, if it fails at the customer site, the customer can send it back. So, we have a product with a thorough process.
From a maintenance standpoint, the poppet cartridge being bottom-loaded allows your key components to be maintained without removing the entire regulator from the system. Since this comes out through the bottom, all we have to do is isolate our pressure upstream, and we can maintain this with a brand-new cartridge.
Our regulators are serviceable. Customers always have the option to purchase spare parts for KPR series regulators and probably more so for the RHPS regulators, which are designed and recognized as serviceable products.
One aspect of regulator quality that isn’t directly tied to the product itself is selection. Proper selection of a pressure regulator can have an outsized impact on not only the performance of the system, but also the longevity of that regulator. The help that Swagelok gives our customers in finding the right regulator for an application can have a very big impact on the performance and outcomes of the fluid systems that our pressure regulators serve.
What sets us apart is the local service and support. We have more than 200 sales and service centers worldwide, and they can offer custom services and support at the local level to help customers meet their needs.