Register - Locate Sales and Service Center
Swagelok® products and services are delivered locally through a network of more than 200 authorized sales and service centers that support customers in 70 countries on six continents.
Home > MPC Configurator

Swagelok Modular Platform Components (MPC) Configurator

MPC Configurator

The MPC Configurator is an interactive tool to build and assemble ANSI/ISA 76.00.02-compliant miniature modular designs prior to the purchase process.

Read the Frequently Asked Questions for the MPC Configurator.

To download and install the Swagelok MPC Configurator:

  1. Please select the version of the MPC Configurator that you would like to download by clicking this link for the 32-bit version: Swagelok MPC Configurator 2.4 - 32-bit or this link for the 64-bit version: Swagelok MPC Configurator 2.4 - 64-bit.
    • The program file is 97 MB.
    • The configurator is in English.
    • The program is a self extracting zip file. Winzip in not needed for the install.
  2. Double click the MPC Configurator Installation file. The install process will begin.
  3. At the MPC Welcome screen, select "Next."
  4. At the License Agreement screen, you will need to Agree to the license agreement and select “Next” to continue.
  5. The installation process will put the MPC configurator files in a folder called "C:\Program Files\Swagelok\MPC Configurator 2.4". If you want to use the default folder, then click the “Next” button. If you want to put the files in a different folder, click "Browse" button and select another folder. When finished, click the “Next” button to proceed.
  6. Click “Next” to start the install.
  7. The files are copied and registered on your computer. The next screen indicates Swagelok MPC setup was completed successfully. Select “Close” to complete the process.

    System Requirements:
    The configurator is in English only at this time.
    The zip file is 97 MB.
    150 MB hard disk space needed.
    Microsoft Windows XP, Microsoft Windows Vista (any version), or Microsoft Windows 7 (any version)
    .NET 3.5.1 Framework
    CAD Output Requirements:
    For AutoCAD Output: AutoCAD 2010 (Lite version will NOT work)
    For SolidWorks output: SolidWorks 2007, 2008, 2009, 2010, 2011, or 2012

 

To run the Web Version of the Swagelok MPC Configurator:

  1. Please read the System Requirements listed below to make sure that your system meets the requirements to be able to run the Web Version of the MPC Configurator.

    System Requirements:
    The configurator is in English only at this time.
    Microsoft Windows XP, Microsoft Windows Vista (any version), or Microsoft Windows 7 (any version)
    .NET 3.5.1 Framework
    Internet Explorer 6, 7 or 8

  2. Click here to run the Web Version of the Swagelok MPC Configurator.

Read the Frequently Asked Questions for the MPC Configurator Web Version.

Log In or Register Now
Register for an account to view pricing, request quotes and order online.
 

Helping you for more than 60 years.


Fluid system training to help you get up to speed quicker.

Locate a Sales and Service Center

Swagelok® products and services are delivered locally through a network of more than 200 authorized sales and service centers that support customers in 70 countries on six continents.

My Location

Loading. Please wait...