Home > IGC II Configurator

Swagelok Integrated Gas Components (IGC II) Configurator

IGC Configurator
 

Our menu-driven software lets you configure on screen, then produces a complete bill of materials with the part numbers along with an assembly schematic.

 

 

 

To download and install the Swagelok IGC II Configurator:

  1. Please download the configurator files by clicking this link: SwagelokIGCIIsetup.zip.
    • The zip file is 12000 KB.
    • The configurator is in English.
    • The files are zipped. You will need Winzip to extract the files.
  2. Use Winzip to extract the setup files. One of the extracted files is called "Setup.exe".
  3. Double click the Setup.exe file. The install process will begin.
  4. The installation process will put the configurator files in a folder called "Swagelok IGC II". If you want to use the default folder, then click the large button located in the upper left of the Swagelok IGC II Setup screen. If you want to put the files in a different folder, click "Change Directory" and select another folder. When finished, click the large button to proceed.
  5. The next screen asks you to select a Program Group. It recommends "Swagelok IGC II". Either accept the default or select another group. Click "Continue" to continue with the installation.
  6. The files are copied and registered on your computer. The next screen indicates Swagelok IGC II setup was completed successfully.

    System Requirements:
    The configurator is in English only at this time.
    The zip file is 12000 KB.
    Winzip is required to unzip the setup files.
    100 MB hard disk space needed.
    Microsoft Windows 98, Windows 2000 or Windows XP operating systems required.

Log In or Register Now
Register for an account to view pricing, request quotes and order online.
 

High value and high performance backed by a limited lifetime warranty.


Quality is a way of life for us.

Locate a Sales and Service Center

Swagelok® products and services are delivered locally through a network of more than 200 authorized sales and service centers that support customers in 57 countries on six continents.

My Location

Loading. Please wait...