Change Language Home Log In Shopping Cart Sales & Service Site Map Contact Us
Fluid System Technologies Search  
Swagelok Integrated Gas Components (IGC II) Configurator

Our menu-driven software lets you configure on screen, then produces a complete bill of materials with the part numbers along with an assembly schematic.


To download and install the Swagelok IGC II Configurator:


  1. Please download the configurator files by clicking this link:  SwagelokIGCIIsetup.zip.
    • The zip file is 12000 KB.
    • The configurator is in English.
    • The files are zipped. You will need Winzip to extract the files.

  2. Use Winzip to extract the setup files. One of the extracted files is called "Setup.exe".


  3. Double click the Setup.exe file. The install process will begin.


  4. The installation process will put the configurator files in a folder called "Swagelok IGC II". If you want to use the default folder, then click the large button located in the upper left of the Swagelok IGC II Setup screen. If you want to put the files in a different folder, click "Change Directory" and select another folder. When finished, click the large button to proceed.


  5. The next screen asks you to select a Program Group. It recommends "Swagelok IGC II". Either accept the default or select another group. Click "Continue" to continue with the installation.


  6. The files are copied and registered on your computer. The next screen indicates Swagelok IGC II setup was completed successfully.
System Requirements:
  • The configurator is in English only at this time.
  • The zip file is 12000 KB.
  • Winzip is required to unzip the setup files.
  • 100 MB hard disk space needed.
  • Microsoft Windows 98, Windows 2000 or Windows XP operating systems required.
Swagelok London

Kingley Park
Station Road
Kings Langley
Hertfordshire
England WD4 8GW

44 0 1923 272 000
info@London.swagelok.com


Forgot password?
Forgot username?

Part Number Search
 
Find product information, literature, CAD templates and Sales Drawings.