Change Language Home Log In Shopping Cart Sales & Service Site Map Contact Us
Fluid System Technologies Search  
 
Renewable Energy Starts at Home
Imagine a house that gets all of its energy for heating, cooling, and cooking from batteries that never require changing – batteries as reliable as the sun. That’s the way Mike Strizki describes the system he uses at his home in Hopewell, N.J.Hydrogen Fuel Cell Powered Home

In fact, the sun is a key player in Strizki’s home. Sunlight energizes the 56 solar panels that provide energy to his 3,000-square-foot house. More than half of the energy collected by the panels is converted to hydrogen, the element that makes up 75 % of the sun’s composition. So while the solar panels are providing energy to the house when the sun is shining, hydrogen is simultaneously being stored for use in cloudy weather.

Strizki’s home is the first of its kind – an existing home, retrofitted for self-sufficient solar and hydrogen power – and, he believes, the first of many to come. Everything in the house runs on electricity and needs no external power supply.

Getting Involved Hydrogen Fuel Cell Power Control Box
Swagelok became involved in the project when Tracey Simpson, owner and president of Penn Fluid System Technologies (Penn FST), the authorized Swagelok sales and service center in Huntingdon Valley, Pa., heard about Strizki’s plans.

“When I spoke to Strizki and he described his project in detail, I saw it as an opportunity we couldn’t pass up,” Simpson says.

Strizki already had his solar panels, storage batteries, hydrogen electrolyzer, generator, and tanks, but not the connection equipment nor the expertise to tie it together. Penn FST provided the equipment – including all points of connection and all of the fluid controls – as well as the assistance to pull it together as efficiently as possible.


Shedding Light on Residential Hydrogen Heating
The Solar-Hydrogen Residence works like this: Photovoltaic solar panels absorb sunlight, converting its energy into electricity. During the sunny months, this electricity heats, cools, powers appliances, fills the hot water tank, and provides energy to cook. At the same time, though, 60 % of the electricity is diverted to an electrolyzer that pulls hydrogen from water. This hydrogen is stored on Strizki’s property in 10 1000-gallon tanks, which employ Swagelok® fluid system components. When energy from the stored hydrogen is needed, the hydrogen flows to a fuel cell where it is converted back into electricity.

Swagelok components and expertise keep Strizki warm in his Solar-Hydrogen Residence in the winter and cool in the summer, all without relying on the traditional power grid nearly every other home in the country depends on. His monthly utility bill? Zero.

In all, Swagelok provided 300 feet of 1/2-inch tubing, 16 AFS ball valves, 10 pressure gauges, and many other components to the Solar-Hydrogen Residence, plus subassembly on two control panels used for controlling the system.

Swagelok Company’s reputation made it easy for Strizki’s home to be approved by building code inspectors. “The involvement of Swagelok went a long way in getting the backing of the inspectors,” Strizki says.



Find a Sales & Service Center



Hose Products and Assemblies
Flexible hose products from Swagelok offer flexible solutions for fluid handling.