Adding flexibility to fluid
       system solutions
Select a Sales and Service Centre
Swagelok New Zealand

About Swagelok

Swagelok manufactures tube fittings, valves, regulators, hoses and other products that are vital to fluid system solutions in industries such as power generation, oil and gas production, chemical processing, biopharmaceutical, research, semiconductor manufacturing and more. Over 200 global sales and service centers support customers using our products.

How we work is as important as what we do. Our corporate values of Customer Focus, Quality, Integrity, Respect, Continuous Improvement and Innovation are lived each day they are not just writing on the wall. We use these values as guideposts in all we do from recruiting new talent, to developing exciting new products, to creating new ways to bring value, and peace of mind, to our customers.


When you need hose, simply call Swagelok. Surprised? Believe it. Swagelok offers a broader range of hose than you may realise-from the toughness of all-metal stainless steel hose to the easy flow of PTFE-lined smooth bore or easy flexibility of PTFE-lined convoluted-bore hose reinforced by stainless steel or synthetic braid in the lengths you need.

Depending on hose type, pressure ratings range from vacuum to 3500 psig (241 bar). Sizes range from 1/8 to 2 in. (3.2 to 50.8 mm) with a wide choice of end connections, including pipe, tube, sanitary, flare, and pipe flange.

And you can choose Swagelok hose that can be autoclaved and sterilised, or built with silicone covering, or constructed with a nonconductive core for applications that require static dissipation.

If you would like further details on the Swagelok Hose and Flexible Tubing range or to discuss a specific application solution, please contact the authorised Swagelok Sales and service centre in your area.

Click here to view the Hose and Flexible Tubing from Swagelok.