New Swagelok® Orbital Welding Power Supply Is Easy to Operate, Packs a 200 Amp Punch
SOLON, Ohio (November 15, 2007) Swagelok Company announces the release of the new Swagelok® welding system M200 power supply that offers ease of use, portability, and 200 amp capability, all at a weight of less than 50 lbs. (23 kg).
A high-resolution, 12.1 in. (307 mm) color industrial touch screen gives users a simple, intuitive pathway to enter weld programs. Users can choose from one of three forms to enter weld programs, including automatic weld schedule programming. The M200’s automatic shield gas control (patent pending) simplifies set-up of shielding gas, requiring no use of a separate flow meter.
Multi-language capability is built in to the M200, requiring no separate programming or special ordering. Built-in languages are English, French, German, Spanish, Japanese, Korean, and Chinese (simplified and traditional). Universal voltage input (100 to 230 V [ac]) requires only a cord/plug change to accommodate an input voltage.
The M200 works with all currently available Swagelok weld heads. It includes four USB ports, Ethernet port, USB device (output) port, VGA output, and serial port. All gas and electrical connections, plus the integral, high-speed thermal printer are easily accessed from the unit’s side panels.
Headquartered in Solon, Ohio, U.S.A., Swagelok Company is a major developer and provider of fluid system solutions, including products, assemblies, and services for the research, instrumentation, pharmaceutical, oil and gas, power, petrochemical, alternative fuels, and semiconductor industries. Its manufacturing, research, technical support, and distribution facilities support a global network of more than 200 authorized sales and service centers in 57 countries. For more information about Swagelok, visit the company’s Web site at www.swagelok.com.
|