You can choose to view this content in a different language by clicking on the specific ISO Language Code.

Customer Testimonials

Sometimes it helps to see that others have had success with our products in a given application to give you the added confidence you may need to rely on our company to fulfill your fluid system product requirements. What follows are many different types of applications where our customers have had success in using Swagelok® products. We have kept the specific contact information for each given customer anonymous. If you would like to discuss the specifics of a particular application with our customer, it is likely that we can arrange a conference call or a personal visit to discuss the application in further detail.

 

 Automotive            High Purity            Power            Small Bore

 

 

 

Automotive

 

Automotive Application 1

Products: Swagelok Tube Fittings
Result: Proven reliability and integrity of connections ensure a leak-tight system.

 

  

 

Products: Swagelok Specially Cleaned Tubing
Result: Tubing cleaned to customer specifications allows customer to benefit from single source purchasing of both fittings and tubing. 

 

  

 

Automotive Application 2

Products: Swagelok Tube Fittings
Result: Customer installed Swagelok tube fittings after they had reccurring problems with pipe end connections leaking at 2000 psi. The system was installed in half the amount of time it took before.

 

  

 

Products: Swagelok Tubing and Supports
Result: Tubing was easily bent and the use of tube supports absorbs vibration, reduces stress on system components and enhances system reliability. 

 

  

 

Automotive Application 3

Products: Swagelok Tubing Fittings
Result: Swagelok tube fittings were chosen as a leak-tight solution for this application with vibration and pulsating hydraulic fluid in system.

 

  

 

Products: Swagelok Needle Valve
Result: High pressure needle valves are used to isolate and control flow during testing. Also, the integral Swagelok ends allowed the customer to position the valves in the most desirable orientation. 

 

  

 

Products: Swagelok Gauges
Result: Panel mounted gauges helped to facilitate the installation and are manufactured in accordance with ASME, EN and JIS standards. Every Swagelok industrial pressure gauge is factory calibrated and pressure tested. 

 

  

 

 

High Purity

 

High Purity Application 1

Products: Swagelok® Sanitary Fittings
Result: The use of the Swagelok Welding System allowed the contractor to increase welding output to almost 80 welds per day. Swagelok also provided specially configured fittings, saving the contractor valuable time while on the job. 

 

  

 

High Purity Application 2

Products: Swagelok Micro-Fit® Weld Fittings and Swagelok VCR® Metal Gasket Face Seal Fittings
Result: Swagelok Micro-Fit weld fittings allowed our customer the ability to reduce the overall footprint of their system. The cleanliness level of the Micro-Fit weld fittings was also a determining factor in the decision to use these products. Swagelok VCR metal gasket face seal fittings offered the customer proven reliability. In addition, zero-clearance connections allowed easy component removal. All connections were installed with the Swagelok Welding System. 

 

  

 

Products: Swagelok Diaphragm Valve
Result: High purity valves were used because of their high integrity and cleanliness. In addition, these valves also offered the option of valve position indicators on the handles. 

 

  

 

 

Power

 

Power Application 1

Products: Swagelok® Tube Fittings
Result: Swagelok thermocouple fittings are used to relay temperature and pressure of gases back to the control room. This information is critical to the everyday operation of the plant. 

 

  

 

Products: Swagelok Tube Fittings
Result: Field threading can produce threads of widely varying quality and finish along with high scrap rates. Assembling tapered pipe threads means turning a length of pipe or an entire fitting, making alignment haphazard and time consuming. In addition, a sealed pipe joint subject to vibration as well as temperature and pressure extremes may begin to leak after a period of time.

Swagelok tube fittings are routinely installed in half the time as piping systems, allowing for the use of fewer connections and therefore fewer potential leak points.

 

  

 

 

Small Bore

 

Small Bore Application 1

Products: Swagelok® Tube Fittings >1”
Result: Customer used carbon steel Swagelok tube fittings on hydraulic lines. The engineer wanted the ability to maintain flow without installing elbows.

 

  

 

Small Bore Application 2

Products: Swagelok Tube Fittings >1”
Result: Equipment manufacturer had reoccurring problems with black pipe leaking on high pressure hydraulic lines. Swagelok tube fittings were installed using a Swagelok Hydraulic Swaging Unit (HSU). This tubing system was installed in half the time it took to install the black pipe. 

 

  

 

Small Bore Application 3

Products: Swagelok Tube Fittings >1”
Result: This research facility used Swagelok tube fittings to install a small bore system using copper tubing. The installation time was significantly reduced, and the elimination of contamination associated with a soldered system afforded them the cleanliness they desired.

 

  

 

Small Bore Application 4

Products:  Swagelok Tube Fittings - 1/2" & 1"
Result:  Performing onsite HSU training assured the customer safe, reliable installation of  this helium application.  With over forty stainless steel 1" Swagelok connections and thirty stainless steel 1/2" Swagelok connections, not one leak was found when tested at over 2500 psi, over-night.  The customer also verfied that that the system operated over 3000 psi with no known leak.

 

  


 

 

       

        H. E. Lennon, Inc.  -  248-474-6624  -  info@lennon.swagelok.com

 

Helping you for more than 60 years.


Our systems work with your systems.


VISIT US ON

Locate a Sales and Service Center

Swagelok® products and services are delivered locally through a network of more than 200 authorized sales and service centers that support customers in 57 countries on six continents.

My Location

Loading. Please wait...